Tip: Only prices matching all the settings above are included in the report. Conflicting settings, such as State limited to Victoria and Site limited to Port Adelaide, will cause no prices to be displayed.
Set which prices are included in this report by editing one or more of the settings in the Customise This Report section. Use Save Report Settings to name and save the current report setup. You can then create an updated version of this report at any time from the My Reports page. Use Print Report to display and print a printer-friendly version of this report. Use Download Results to create and store (on your computer) a CSV file containing the data in this report. A CSV file can be imported into many spreadsheet and database programs.
- At Viterra and ABA sites, all prices are exclusive of storage and handling charges. Prices are quoted at base grade quality, exclusive of GST. All prices are subject to change or withdrawal without notice.
- The "Quality Scales" column should be interpreted as follows: "Yes" means quality scales do apply and will affect the price paid by the buyer; "No" means that quality scales are not applicable.
- When shown, the "Quality Adjustment" column shows a premium or discount that is calculated from the test results you have entered and the applicable quality scales supplied by the marketer. If you do not enter any test results, or the marketer has indicated that quality scales do not apply, the Quality Adjustment is zero. If a marketer has indicated that quality scales apply to a price but that marketer's applicable scales are not known to ezigrain, a question mark is displayed.
- When shown, the "Quality Adjustment" column shows a premium or discount that is calculated from the test results you have entered and the applicable quality scales supplied by the marketer. If you do not enter any test results, or the marketer has indicated that quality scales do not apply, the Quality Adjustment is zero. If a marketer has indicated that quality scales apply to a price but that marketer's applicable scales are not known to ezigrain, a question mark is displayed.
Please note that all prices and quality scales are provided by outside parties. Should the seller rely on the prices and quality scales provided, the seller does so at its own risk and acknowledges that ezigrain does not represent or warrant that the figures provided or the results generated are accurate. It is the grower's absolute responsibility to confirm Quality Scales, conditions of any purchase option type and actual price (including any other fees, levies, royalties or charges applicable) with the buyer. Please note that "Price Less Fees" may not ultimately be the actual price. Growers should fully inform themselves when making marketing decisions.
Please contact the Viterra Customer Service Centre on 1800 018 205 or your grain marketer should you require further assistance